2019-07-22 4:38 AM
When I connect the two pads at the PCB, routing under the module, TCXO_VDD will have a voltage of 0.8, irrespective of whether PA12 is high or low. In fact, I have only found it by taking the cover of the module and find a capacitor pad where TXCO is connected.
When set to high, the track voltage will spike for a few nanoseconds and then quiesce again to the 0.8 V level.
I am trying to solve the situation by routing from outside the module, like we can find at the LRWAN1 development board. Will it be enough or is there some sort of a weird module quirk I have to consider?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.