2025-10-07 3:26 PM - last edited on 2025-10-08 1:06 AM by Imen.D
There is an error in table 17 on page 33 in regards to two of the pin positions for the MB1880A adapter. Table 17 states that pin 2 is SPI1_MOSIP (PA7) / UART1_TX (PC1) and pin 3 is SPI1_MISOP (PA6) / UART1_RX (PC0). These two pins are reversed in both the CN2 and CN3 columns.
In actuality, pin 2 is SPI1_MOSIP (PA7) / UART1_RX (PC0) and pin 3 is SPI1_MISOP (PA6) / UART1_TX (PC1).
This is confirmed by table 13 (page 28), the MB1779 schematic (MB1779-HIGH-BAND-B02 Board schematic under the B-WL5M-SUBG1 CAD Resources tab), and wasting an hour trying to determine why the I2C3 port was not talking to a device.
Solved! Go to Solution.
2025-12-11 12:29 PM
Hello All,
This issue is fixed in the latest release UM3127 Rev4.
Thank you for your contribution.
2025-10-08 12:43 AM
2025-10-08 1:03 AM
Thank you for bringing this to our attention.
An internal ticket number 219127 is submitted in order to fix this error in the coming releases of UM3127.
(PS: Ticket number 219127 is an internal tracking number and is not accessible or usable by customers).
2025-12-11 12:29 PM
Hello All,
This issue is fixed in the latest release UM3127 Rev4.
Thank you for your contribution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.