cancel
Showing results for 
Search instead for 
Did you mean: 

Decoder for LoRa messages for Datacake

MihaiMEC
Associate

Hello,

I followed the indtructions from here, https://www.youtube.com/watch?v=vuc6914B0KM and I setup the NUCLEO-WL55JC STM32WL Nucleo-64 board and sensor board X-NUCLEO-IKS01A3 with LoRaWAN Gateway P-NUCLEO-LRWAN2 through The Things Network (TTN).

In this moment I am able to see the raw data in TTN Live data watch.

In the youtube 5 video example, the autor use the Cayenne app to create dashboard in order to decode and siaplay the sensor data.

Now, the issue is this: Cayenne is no more available, could you provide a Decoder code in JSON format for uplink and downlink, for application example LoRaWAN_End_Node?

Thank you,

Mihai

1 REPLY 1
STTwo-32
ST Employee

Hello @MihaiMEC 

No need for a modification on the Code of the LoRaWAN_End_Node. You can keep using the DATACAKE for example or the Zafron platform that can receive the same data frame as on Cayenne. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.