2022-03-06 9:28 AM
Hello,
I would like to transfer data between two P-NUCLEO-WB55 boards. I took a look at the p2p-Server/Client example and I think this is just what I need. I used the project templates from CubeIDE and created two own versions. For this I followed this tutorial and got both server and client running. For the server I managed to change the attribute value. Now I would like to establish a connection between both boards. How can I establish a connection and maybe filter for specific devices in my application?
2022-04-07 2:05 AM
Hello,
If you take BLE_p2pServer and BLE_p2pClient example from STM32CubeWB package, you have the following behavior:
- The Peripheral device (BLE_p2pServer) starts advertising (during 1 minute), the green led blinks for each advertising event.
- The Central device (BLE_p2pClient) starts scanning when pressing the User button (SW1) on the board.
- BLE_p2pClient blue led becomes on.
- Scan req takes about 5 seconds.
- Make sure BLE_p2pServer advertises, if not press reset button or switch off/on to restart advertising.
- Then, it automatically connects to the BLE_p2pServer.
- Blue led turns off and green led starts blinking. Connection is done.
You can look Event_Handler function in BLE_p2pClient example, in p2p_client_app.c file, to see how the connection is filtering for a specific device (here P2P_Server).
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.