2020-01-28 6:12 AM
Is it possible to get connection with several smartphones on the STM32WB?
As I understand the STM32WB can connect several servers but not clients (smartphones), or I got it all wrong?
Thanks,
Lior Malik
2020-01-29 5:37 AM
There is no restriction at GATT level (Client/Server architecture).
The STM32WB can support up to 8 connections but only 2 slaves at Link layer level (GAP level).
2020-01-29 5:58 AM
thank you for your response.
is there any example that support several connections?
2020-01-29 9:24 AM
Please have a look the STM32Cube_FW_WB_V1.4.0\STM32Cube_FW_WB_V1.4.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pRouteur project.
Go to the readme.txt file
demonstrate STM32WB55xx capabilities:
-- 1 slave & 6 masters connections on same device
-- GATT Server & GATT Client on same device
-- Automatic reconnection
-- Special Advertising format is proposed
-- Proprietary Services & Characteristics are used
2020-01-30 3:33 AM
Thank you very much.
I will look at this one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.