2024-12-24 2:01 AM
Hello there,
I'm trying to execute the BLE_HeartRate Service example on WB55rg Nucleo board. Initially I successfully run the code.
Later I'm trying to download the same code again BUT I'm getting following message repeatedly in the CONSOLE:
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying..
Also, bi-color LED i.e. LED6 on the board is not turning RED at the end.
I tried executing my other projects and all are downloaded properly with last message as:
Download verified successfully
Shutting down...
Exit.
BUT Why this BLE_HeartRate is creating an issue, I'm unable to figure out.
Your help is very much appreciated.
Thank You.
Solved! Go to Solution.
2024-12-24 4:33 AM - edited 2025-01-30 9:38 AM
Hello @OS_Er
On the app_conf.h file, set the following definitions:
#define CFG_DEBUGGER_SUPPORTED
#define CFG_DEBUG_BLE_TRACE
#define CFG_DEBUG_APP_TRACE
to 1:
#define CFG_DEBUGGER_SUPPORTED 1
#define CFG_DEBUG_BLE_TRACE 1
#define CFG_DEBUG_APP_TRACE 1
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-24 4:33 AM - edited 2025-01-30 9:38 AM
Hello @OS_Er
On the app_conf.h file, set the following definitions:
#define CFG_DEBUGGER_SUPPORTED
#define CFG_DEBUG_BLE_TRACE
#define CFG_DEBUG_APP_TRACE
to 1:
#define CFG_DEBUGGER_SUPPORTED 1
#define CFG_DEBUG_BLE_TRACE 1
#define CFG_DEBUG_APP_TRACE 1
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.