2024-08-09 5:18 AM - last edited on 2024-08-09 8:23 AM by Amel NASRI
I need to program the Nucleo-wl55jc1 for work to send data via LoRa. I followed the stm tutorials and connected successfully to the lora chirpstack server. The first connection worked fine, but when reseting the nucleo, it gives some nonce error because I think the nonce value is not storred correctly in flask memory upon successful join. I searched 2 days on the internet and looking trouth the code, but unsuccessfull. Now, to take a break from this, I want to send data on the first successful join, after reseting server nonce. I found the ping pong example, but I don`t understand it well, and I want sonething like a function to send hex data via LoRa. After I have that function made, I can decode the I2C data from another sensor and send it`s data via lora once every 8h.
2024-08-28 3:15 AM
Hello @Tonikiller10000
First, The PingPong application is not a LoRaWAN application. If you are looking for a LoRaWAN application to send data From I2C to Your board and then to a LoRaWAN network, please follow the implementation available on the videos 3,4 and 5 of this Playlist.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.