2024-08-28 6:19 AM
I've got custom hardware with an STM32WB5MMGH6 micro. I am using STM32CubeIDE Ver 1.16.0.
I fetched the BLE_Sensor project to use as a code base for development. I edited the IOC and removed a lot of the peripherals that don't exist on my hardware. I loaded the BLE Stack (stm32wb5x_BLE_Stack_full_fw.bin) into the RF co-processor. I built and loaded the modified BLESensor App (which I 'renamed' to Cardinal). When I run the code, it ends up stuck in the USB_LP_IRQHandler. The NVIC says this interrupt is not enabled. I attached a screenshot of the IDE showing the Debug call stack, C file, and Disassembly windows. Is it a coincidence that the IRQ is 4 bytes before the Main function entry point? And what's with the <signal handler called>() at 0xffffffff9 seen in the call stack?
Any ideas on why I'm getting stuck in the USB_LP_IRQHandler?
2024-09-20 11:31 AM
Hello @JimEno
Are you sure is not a HW issue. Could you please check this.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.