2024-07-29 2:42 AM - edited 2024-07-29 3:11 AM
Hi,
We are using BLE central stack,
Version: 1.17
Use case: BLE central on a WB55 node performs device discovery and tries to connect to a BLE device with random address. A typical good flow works very well, central connects and read out all characteristics. But as the BLE device is battery powered and sometime goes to sleep. When BLE device is in sleep mode (after advertising for certain duration) and if BLE central tries to connect this sleeping device, the connection timeout event (or any such event with HandleHciLeConnectionUpdateCompleteEvent) is not raised by stack. All further calls to API
auto peerAddress = RANDOM_ADDR;
// Create connection parameters
const uint16_t leScanInterval = 0x320;
const uint16_t leScanWindow = 0x320;
// Connection Interval parameters
const uint16_t minConnectionEventLength = 0;
const uint16_t maxConnectionEventLength = 0x280; // 400 ms
// Terminate connection
const uint8_t remoteUserTerminatedConnection = 0x13;
uint16_t minConnIntMultiplier = 6; // 7.5 ms
uint16_t maxConnIntMultiplier = 6; // 7.5 ms
uint16_t slaveLatency = 0;
uint16_t supervisorTimeoutMs = 50; // 500 ms
aci_gap_create_connection(
leScanInterval, leScanWindow, peerAddress, macAddress.data(), RESOLVABLE_PRIVATE_ADDR,
minConnIntMultiplier, maxConnIntMultiplier,
slaveLatency, supervisorTimeoutMs,
minConnectionEventLength, maxConnectionEventLength);
2024-07-29 3:04 PM
Hi All,
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Jake
ST Support
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.