2025-07-10 2:48 AM
why don't have GCC file when the stm32cube MX create project of touchGFX, but
ST official project have this ?
2025-07-10 6:28 AM
Hello @miker,
Please avoid spamming threads on the forum. Before starting a thread, please refer to the documentation first to see if you can find an answer to your issue, or search in the forum to see if somebody had the same issue as yours.
You have the TouchGFX documentation with example, article and tutorial here TouchGFX Documentation | TouchGFX Documentation.
It's because it was generate with TouchGFX Designer, yours was generated with CubeMX. These 2 tools are different.
BR,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.