2025-09-25 2:09 AM
I'm using NemaGFX on the STM32U5G9J-DK2 kit without RTOS and without TouchGFX, which works very well.
I've created lightning-fast graphical widgets on that kit.
Now I have an STM32H7S78-DK and I'm having trouble getting *all* NemaGFX functions to work properly.
Many functions work properly, but the functions that draws filled circles and shapes with rounded corners still have problems. Maybe I'll get it working later.
So I thought TouchGFX might be useful for initializing NemaGFX on this kit, and then using its functions to create my own graphical widgets.
So I created a project with 4.26.0 that only displays a button on the screen to confirm it's running on the target.
Then I looked at the generated code and, to my surprise, no NemaGFX functions were revealed.
Does it actually use GPU2D and NemaGFX? Why isn't it showing up? I'm a bit worried that I can't use the NemaGFX library with TouchGFX.
If that's the case, TouchGFX is useless to me.
How do I use the NemaGFX library within a TouchGFX project?
I want to display my own graphical widgets without the limitations of TouchGFX.
Is that possible?
2025-10-14 7:31 AM
Hello @Jack3 ,
Yes, touchgfx uses NemaGFX with some abstraction (check Middlewares/ST/touchgfx_components folder).
You can use NemaGFX directly in touchgfx in different ways, for example you do all you drawings in a dynamic bitmaps that you set as the dst texture.
Another example here Solved: LTDC Rotation 180 degres - STMicroelectronics Community I use the nema library to do a 180 rotation of the whole Framebuffer.
BR,
2025-10-22 11:44 PM - edited 2025-10-22 11:52 PM
Well, it turns out I couldn't succeed using NemaGFX, making the use of TouchGFX pointless for me.
Any practical examples of using NemaGFX in a TouchGFX project or practical directions will be welcome.
2025-11-13 2:25 AM
Hello @Jack3.
In the thread Louis has linked to in his latest answer, there is an example of using NemaGFX in a TouchGFX project.
See the TouchGFXHAL::endFrame() function in Appli\TouchGFX\target\TouchGFXHAL.cpp.
Best regards,
Johan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.