2019-11-18 5:24 PM
I check yes and everything appears to work.
What is the GFXSIMULATOR mode and can I deselect it in the Pinout & Configuration tab?
I see the generated code in main.c calls a generated init function, but it is empty except for comments delineating user code sections.
When I select Pinout & Configuration tab -> Application -> GFXSIMULATOR, it says the FAHB (MHz) is configured for 180 but the simulator is 168. All the other configuration settings match the simulator settings. I suspect this is the cause of the popup. But I want to run at 180. How should I proceed?
Thank you,
2020-01-09 12:38 AM
GFXSIMULATOR is unrelated to TouchGFX, so disabling it is fine. How did you create the project? It's not something i usually see when creating TouchGFX projects in CubeMX. Did you try the new 5.5.0 combined with TouchGFX 4.13.0 ?
/Martin
2020-01-10 6:14 AM
I'm not using Touch GFX and I don't want to use GFXSIMULATOR. How do I disable it in STM32CubeMX?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.