2022-07-21 10:48 AM
Hi All,
Are there any TouchGFX examples driving multiple displays over SPI using ILI9341 controller? I am able to drive a single 320x240 display no problem but run into issues when extending to two displays.
I'm guessing I am sending too much data over SPI but I am assuming that each SPI controller is independent so data sent over SPI1 should not affect data sent over SPI2?
I am using the following components:
ST NUCLEO-F767ZI
STM32CubeIDE v1.10.0
TouchGFX Designer 4.20.0
2.4" DisplayTech TFT (DT024CTFT) using ILI9341 Controller
Thanks,
Mike
2022-07-24 10:13 PM
2022-07-25 1:11 PM
The mirroring is just for testing. I needed something simple to test driving two displays. You are correct. Eventually I will have independent data going to both displays. The plan is to extend the H.
Thanks for the suggestion. I will try reordering the commands in the transmit block. Yes. The set commands are not using DMA, just the pixel data.
2022-07-25 10:07 PM
2022-07-26 10:48 AM
Thanks again for your continued support. Any suggestions on how to improve upon waiting for two callbacks?
I have optimized the ILI9341_SetWindow and ILI9341_DrawBitmap to combine SPI1 and SPI2 with little improvement.
Is there another LCD controller you would recommend? I have searched for others and have found slightly faster serial write cycle of 66ns...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.