2024-11-09 6:21 PM
I have created a project with a scroll wheel of 10 items, each item is displaying a single digit 0-9. Imagine an odometer for instance. I am incrementing a variable(num) every second and using
scrollWheel.animateToItem(num, 20);
to scroll through the list of items, it is working as expected until it gets to 9. Instead of it the scroll wheel continuing to rotate the same direction to 0 it reverses the direction of rotation and scroll past all other digits to get back to zero.
I have verified I have the scroll wheel set as "Circular" and it does indeed display the scroll wheel correctly as if it was circular. Can I somehow change this behavior?
2024-11-10 12:01 AM
Try combine with
| virtual void | animateToPosition(int32_t position, int16_t steps =-1) |
2024-11-10 4:42 AM
You can use the modulus operator to calculate which item to display while keeping a continuous count for num so that the scroll wheel always has a “forward” motion.
let num = 0;
setInterval(() => {
scrollWheel.animateToItem(num % 10, 20);
num++; // Keep incrementing num indefinitely
}, 1000);
2024-12-13 7:36 PM
I want to revisit this issue with a better explanation and more details.
I have a circular scroll wheel with 10 elements, each element is displaying a single number 0-9. If I set the scroll wheel in code by callingscrollwheel.animateToItem(9, 20); and then call callingscrollwheel.animateToItem(0, 20); the wheel will animate from scrolling all digits from 9 down to zero.
But if I reverse the order of the calls, callingscrollwheel.animateToItem(0, 20); and then callingscrollwheel.animateToItem(9, 20); the scroll wheel acts as expected and will animate directly from 0 to 9.
This appears to be a bug to me as the circular scrollwheel is only behaving as a circular wheel in one direction where animating in this order 2, 1, 0, 9, 8...works as expected, and animating from 8, 9, 0, 1, 2 does not act like a circular wheel.
If I change the scrollwheel to not be circular if will always scroll through all digits when going from 0 to 9 and also when going 9 to 0.
2024-12-13 11:10 PM
You little miss idea. TGFX is TOUCH primary and circular here mean both direction work neverending...
Code control is other species.
2026-04-23 3:01 AM
I have the same problem, did you find any solution?
2026-04-23 8:40 AM - edited 2026-04-23 8:41 AM
If you use without touch try add 0 to end 0,1,2,3,4,5,6,7,8,9,0 and split scroll negative to scroll to item 11, switch to item 0 and scroll to target... Or complete twice 0-9 0-9 ...
2026-04-23 10:43 PM - edited 2026-04-23 10:45 PM
Yes, I don't have a touch screen and only use physical buttons. After replying to this post, however, I tried something "no sense" that seems to work, namely:
//UP
int currentIndex = scrollWheel1.getSelectedItem();
scrollWheel1.animateToItem((currentIndex + 1), 5);
//DOWN
int currentIndex = scrollWheel1.getSelectedItem();
scrollWheel1.animateToItem((currentIndex - 1), 5);
I'm not interested in pushing the limits in either direction and "strangely" everything works without generating any graphical glitches.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.