2023-10-24 1:44 AM - edited 2023-10-24 2:35 AM
Hello All,
I have set XPT2046 and set sample touch as specified by the documentation and I have getting coordinates accordingly but the problem is when I try to press the button I register the X, and Y coordinates but there is a delayed response, or the key is registered but touch gfx doesn't process forward.
Touch Strokes are working fine when touch is pressed according to Debugger.
CHECK THE VIDEO LINK BELOW FOR CLARIFICATION
2023-10-30 8:52 AM - edited 2023-10-30 8:56 AM
This is the final routine that I am using
bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y)
{
if (XPT2046_TouchPressed()) {
XPT2046_TouchGetCoordinates((uint16_t*) &x, (uint16_t*) &y);
x_axis=x;
y_axis=y;
return true;
}
return false;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.