2020-11-13 1:25 AM
Hi,
I am new to the TouchGFX library and trying to make it work with the STM32F429-DISC1 board. The touch display is working fine and I don't see any issues with it. I am now trying to work around the Hardware Button to work with the TouchGFX library.
On the board there is a PUSH button and I want to make it work with the screens. I know there is a workshop available for the Hardware button and TouchGFX interface.
Is there any example available to work with the Push button or Hardware Buttons with the TouchGFX library or any resources?
I would appreciate your help.
Thanks
Azeem
2020-11-14 5:44 AM
Sorry @Michael K , maybe im defense, but not to you , better is say to TouchGFX maintainers ( when you arnt :) ). And as you write complex examples is for C++ experts and Designer is for users without this knowledge. Then i mean simplest way is simply simples and for more complicated Interactions you dont need 15 or 30 , you can use one and set NEW VIRTUAL FUNCTION and this write manualy only inj View. And of course you have right, that exist project where you need Model - Presenter - View communicate, but real user need to know, that Model class exist in TouchGFX only in one instance ...
2020-11-16 9:30 PM
Hello AMuha.1,
You can take a look at the G071-NUCLEO Application template available in TouchGFX Designer 4.15. This project uses a proper ButtonController class that is used by TouchGFX to check the state of the hardware buttons (in this project case, it's a joystick with 5 states).
The only difference that you will face is that you need to find out which pin you need to look at on the F429-DISCO to get the current state of the hardware button :)
Hope this will help.
/Alexandre
2020-11-17 1:00 AM
Thanks Guys, I will take a look at the above examples. Appreciated
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.