2021-10-14 5:28 AM
Hello,
I have a STM32F723 Application with TouchGFX (4.16.1) Graphics over SPI and a Display with RM69330 Controler (454x454x2Bpp).
I use PartitialBuffer Configuration, because internal RAM is too small for whole Framebuffer. I've implemented the Transmit Function ("touchgfxDisplayDriverTransmitBlock( uint8_t* pixels, uint16_t x, uint16_t y, uint16_t w, uint16_t h)") where I set Position Rectangle in Display Controler and write Pixels to the Display. That works fine if x/y/w/h are a multiple of 2 otherwise it looks weired.
Problem is: In RM69330 DataSheet it says that Column and Row Startaddress and Width / Height "must can be divisible by 2".
Question: Is there any way to tell TouchGFX to only supply framebuffer parts with x/y/w/h as a multiple of 2? Or is there any other Known solution?
Solved! Go to Solution.
2021-10-19 12:54 AM
Hello IHei?,
This problem can happen and we discovered this is a common limitation for several SPI displays.
To fix it, you have to modify FrontendApplication.hpp and .cpp as below :
FrontendApplication.hpp
virtual void draw(Rect& rect);FrontendApplication.cpp
void FrontendApplication::draw(Rect& rect)
{
if (drawCacheEnabled)
{
Rect even(rect);
//ensure start x is even number, or move left
if (even.x&1)
{
even.x--;
even.width++;
}
//ensure width is even number of pixels
even.width = (even.width+1)&~0x01;
//ensure start y is even number, or move up
if (even.y&1)
{
even.y--;
even.height++;
}
//ensure height is even number of pixels
even.height = (even.height+1)&~0x01;
Application::draw(even);
}
else
{
Application::draw(rect);
}
}You basically overwrite the draw function to ensure even numbers for the rectangle to draw.
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2021-10-14 8:29 AM
Maybe you can in your transmit function extend x,y,w,h to multiple 2 with read data from display , but yes this is more overhead as send only.
2021-10-19 12:54 AM
Hello IHei?,
This problem can happen and we discovered this is a common limitation for several SPI displays.
To fix it, you have to modify FrontendApplication.hpp and .cpp as below :
FrontendApplication.hpp
virtual void draw(Rect& rect);FrontendApplication.cpp
void FrontendApplication::draw(Rect& rect)
{
if (drawCacheEnabled)
{
Rect even(rect);
//ensure start x is even number, or move left
if (even.x&1)
{
even.x--;
even.width++;
}
//ensure width is even number of pixels
even.width = (even.width+1)&~0x01;
//ensure start y is even number, or move up
if (even.y&1)
{
even.y--;
even.height++;
}
//ensure height is even number of pixels
even.height = (even.height+1)&~0x01;
Application::draw(even);
}
else
{
Application::draw(rect);
}
}You basically overwrite the draw function to ensure even numbers for the rectangle to draw.
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.