2023-10-30 6:49 AM
Hello,
I have a .png image that I'm using in the TouchGFX GUI (utilizing the STM32H725AGI6), which I have fully integrated with the display and working.
That image is going to dynamically change based on a specific value received from the code (0-100%). When it's 100%, the entire image is showing. When the value is 50%, the left half of the image is revealed and the right half will not be shown. When the value is 0%, the image is not showing.
I was previously using a black box that was on a layer higher than the image and had it slowly cover it, but now I have a real background image and not a black box, so that is no longer feasible.
Is there a way to dynamically define how much of the image is drawn? Something similar to the image below.
Solved! Go to Solution.
2023-10-30 11:47 AM
2023-10-30 11:47 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.