2020-09-08 3:50 AM
Hello,
I am working on a project with stm32f769i-eval and touch gfx designer(4.13.0) .
I select my board as application template then I try both using a blank template or any of the examples that are provided.
After generating the code, I try to run the project on my target and even though it doesn't fail my screen is not displaying anything. (If I run on the simulator it works perfectly).
What should I do?
Thx,
Irene
Solved! Go to Solution.
2021-06-01 6:17 AM
The workaround is working for me. Thank you very much.
Good luck further investigating!
Regards,
Tim
2021-06-01 6:21 AM
thanks ;) Good luck with your project
2021-06-27 4:20 AM
Hi @Romain DIELEMAN ,
I had the same problem, and your workaround worked for me. But isn't there a formal fix yet? I'm using TouchGFX Designer 4.16.1.
Thanks
2021-06-30 2:07 AM
Hi,
There should be a fix soon. It will most likely be a new application template with the revision specified.
/Romain
2021-07-02 12:50 AM
Actually it will not be a new TouchGFX Board Setup (new name for "Application Template") but just a new version of the existing one for the STM32F769-eval. It should be up next week or the week after.
/Romain
2021-11-12 8:19 AM
*edited*
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.