2025-06-20 8:44 AM
Hi I'm just starting to use TouchGFX designer, with a background in other UI design programs, and one thing I'm frustrated about is the lack of the ability to align and distribute assets on a screen. I do appreciate the snapping that happens but if I need to distribute a number of objects evenly or just batch align them all with one click, it becomes bit of a pain to manually type x and y locations for each one.
I guess it's not that big of a deal, but just a feature that I feel is missing from a UI design software that others have and feels like TouchGFX is behind in this aspect.
Also there is a bug in 4.25.0 where if you have multiple objects selected and then move them, when you deselect them by clicking elsewhere, the mouse automatically latches to the "box select" mode.
2025-06-23 6:29 AM
Hello @tkuzma ,
Thank you for your feedback, I will inform the team about this feature.
I am not able to reproduce your issue on 4.25.0.
When I select multiple widgets and move then, then I click away from the selected element to unselect them, everything works as expected.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.