2019-12-05 1:23 PM
I am using the function BSP_AUDIO_IN_Record to read audio from line in of this evaluation board.
The data will be used to get a value to display in a Vu-meter so I don't need an extreme precision.
I have add these source in the Makefile to have all functions for this operation.
$(Drivers_path)/BSP/STM32746G-Discovery/stm32746g_discovery_audio.c \
$(Drivers_path)/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sai.c \
$(Drivers_path)/BSP/Components/wm8994/wm8994.c \I have add some includes in these source to eliminate the errors in compile phase.
/* Includes ------------------------------------------------------------------*/
#include "stm32f7xx_hal_dma.h"
#include "stm32f7xx_hal_sai.h"
#include "stm32746g_discovery_audio.h"Here the code:
void Screen2View::setupScreen()
{
#ifndef SIMULATOR
#define MIC_SAMPLES 128
audioBuffer = (uint16_t *)malloc(MIC_SAMPLES * 2);
if (BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 80, AUDIO_FREQUENCY_16K) == AUDIO_OK)
{
BSP_AUDIO_IN_Record(audioBuffer, MIC_SAMPLES*2); <<<< hang here
}
#endif
Screen2ViewBase::setupScreen();
}
2020-01-09 12:20 AM
Hi,
I think i'll need more information to go on. When does the hangup happen? Immediately when the code is executed? Have you tried debugging? What's the application doing when it hangs?
/Martin
2020-01-09 12:24 AM
A side note:
It's better practice to store non-UI related code in the model. Your view has access to its presenter which has access to the model.
View:
presenter->startRecording(MIC_SAMPLES*2);Presenter:
model->startRecording(...);/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.