2023-01-30 6:57 AM
I have a projet with FreeRTOS and FreeRTOS-Plus-TCP working on a STM32F769I-Eval board.
The ICMP Ping response is 100%.
When enabling a TouchGFX application, even very basic (just a white screen), the ping response rate fall bellow 50%! Not usable at all!
Deactivating the TouchGFX application (comment on the line creating the thread) solve the Ping problem.
Is there a compatibility problem with TouchGFX and ETH on the board?
Or does anybody knows what could explain this behavior?
TouchGFX version 4.21, F7 Firmware v1.17.
2023-02-07 9:10 AM
Hello @ANauz.1,
Did you start from scratch (from TouchGFX Designer) or from STM32CubeMX?
It maybe you have an issue with Ethernet/FreeRTOS config! Can you share the settings?
Refer to these posts with Ethernet issues:
Take a look at this video. It might help you.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.