2020-10-26 11:30 PM
Hi,
Is there any Hardware / Development Board with 7" inch TFT RGB with Resistive Touch Screen with SDCard and USB mass storage that support TouchGFX 4.15.
--
Karan
2020-10-30 3:04 AM
Hi, that's a very specific request. The answer is No.
Do you have a specific question in mind?
/Martin
2020-10-30 3:19 AM
Thanks for update..
I have seen most of ST boards has 4.3 inch 480 x 272 resolution with RGB Interface.
I need to connect 7" Inch RGB Interface with Resistive (or Capacitive)Touch and use TouchGFX with that..
Please Guide me.
--
Karan
2020-10-30 4:21 AM
Generally, we do not provide "demos" or "examples" of Board specific features like SD-Cards / FreeRTOS, etc.
You can check the CubeFW pack examples for this and use that functionality with the Application templates in touchgfx.
If you want an example of an RGB Display with resistive touch, check the F429-DISCO Application, specifically how data is retrieved from the touch ic through the TouchController class. Check the CubeFW packs for examples on how to use SD-cards and FreeRTOS.
/Martin
2020-10-30 5:20 PM
Thanks
Any Idea for interfacing 7 inch RGB 800 x 480 Resolution or more with STM32 with or without external frame buffer?
2020-11-02 5:52 AM
What concretely do you mean? What bitdepth? TouchGFX offers various strategies, single fb, double fb, partial fb depending on needs/restrictions.
/Martin
2020-11-02 9:49 AM
Thanks for update...
I have to interface 7 inch TFT 800 x 480 . Bit Depth - 16 Bits
Single Frame Buffer is Sufficient for my Application.
--
Karan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.