2021-07-24 12:48 AM
Hi,
when TouchGFX 4.17.0 is opened I'm getting an error stating no internet connectivity even though my laptop is connected to internet . also in the selection of boards I'm not getting any board option .
thanks and regards
sinduja
Solved! Go to Solution.
2021-09-13 6:15 AM
Hi,
The server is not down at the moment. Could you try to open an internet browser and re open TouchGFX Designer again ?
/Romain
2021-09-13 10:57 PM
Hi,
Please see messages from log file below.
Thanks.
-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Messages from log file (with internet browser open) => error 409:
2021-09-14 07:44:39,835 [1] INFO TouchGFXDesigner.App: Logging configured
2021-09-14 07:44:40,777 [1] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (409) Conflict.
System.Net.WebException: The remote server returned an error: (409) Conflict.
at System.Net.HttpWebRequest.GetResponse()
at System.Net.WebClient.GetWebResponse(WebRequest request)
at System.Net.WebClient.OpenRead(Uri address)
at Utils.WebHandling.WebHandler.RequestWithStringResponse(Uri uri)
2021-09-14 07:44:41,496 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started
2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: ***
2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.17.0
2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.17.0\designer
2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19042.0
2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: de-DE
2021-09-14 07:44:41,502 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :
2021-09-14 07:44:41,502 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: .
2021-09-14 07:44:41,504 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.04084 Full 4.8.04084 ) v4.0 (Client 4.0.0.0 )
2021-09-14 07:44:45,705 [17] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (409) Conflict.
System.Net.WebException: The remote server returned an error: (409) Conflict.
at System.Net.HttpWebRequest.GetResponse()
at Utils.WebHandling.ServerRequest.GetResponse()
at Utils.WebHandling.WebHandler.RequestHeadStatusResponse(Uri uri)
-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Messages from log file (with internet browser closed) => error 407:
2021-09-14 07:39:52,556 [1] INFO TouchGFXDesigner.App: Logging configured
2021-09-14 07:39:53,473 [1] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (407) Proxy Authentication Required.
System.Net.WebException: The remote server returned an error: (407) Proxy Authentication Required.
at System.Net.HttpWebRequest.GetResponse()
at System.Net.WebClient.GetWebResponse(WebRequest request)
at System.Net.WebClient.OpenRead(Uri address)
at Utils.WebHandling.WebHandler.RequestWithStringResponse(Uri uri)
2021-09-14 07:39:54,183 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started
2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: ***
2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.17.0
2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.17.0\designer
2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19042.0
2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: de-DE
2021-09-14 07:39:54,191 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :
2021-09-14 07:39:54,192 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: .
2021-09-14 07:39:54,194 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.04084 Full 4.8.04084 ) v4.0 (Client 4.0.0.0 )
2021-09-14 4:31 AM
Hi,
Can you access this http://sw-center.st.com/touchgfx/pacman/4.17.0/STM32F746G_DISCO/STM32F746G-DISCO_front.png ?
/Romain
2021-09-14 4:34 AM
Yes, I can access this image.
2021-09-15 10:24 PM
Hi,
any idea what causes that error 409?
Thanks.
2021-09-16 1:39 AM
Unfortunately not. Could you try using TouchGFX Designer 4.16.1 ? I suppose you are using a proxy server ? When you open TouchGFX 4.16.1 do you get a pop up message at startup asking for id/password?
/Romain
2021-09-16 2:00 AM
Yes, with version 4.16.1 a popup message appears for proxy login and internet connection then works successfully.
Unfortunately, in version 4.16.1 I cannot find an example configured for STM32H735G-DK evaluation board like in version 4.17.0.
Is such an example also available for 4.16.1?
Thanks.
2021-09-16 2:15 AM
Ok so it is a big issue that will be fixed. In the meantime I will share the tpa for the STM32H735G-DK. You need to unzip it and add it to your C:\TouchGFX\4.17.0\app\packages folder and then open TouchGFX Designer again. Like you said this TBS is not available in TouchGFX 4.16.1
/Romain
2021-09-22 2:15 AM
Hi,
can you please also provide the tpa-file for STM32G071-NUCLEO-DEMO with 240x320 LCD?
I tried to copy the file from TouchGFX Designer 4.16.1 to 4.17.0, but STM32G071-NUCLEO-DEMO is not shown in the boards list under "create new".
Thanks.
2021-09-22 2:29 AM
If it is the demo you are looking for and not the TBS for the STM32G071-nucleo board, then it should be under the "Board Specific Demo" tab in the "Demos" section. But I guess you will face the same issue downloading it. I'll try to find it :thumbs_up:.
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.