2020-11-15 8:02 AM
After a basic modiication in my touchgfx project now the TextKeysAndLanguages.hpp is generate with only null car.
Before
* DO NOT EDIT THIS FILE */
/* This file is autogenerated by the text-database code generator */
#ifndef TEXTKEYSANDLANGUAGES_HPP
#define TEXTKEYSANDLANGUAGES_HPP
typedef enum
{
GB,
NUMBER_OF_LANGUAGES
} LANGUAGES;
typedef enum
{
T_SINGLEUSEID1,
T_SINGLEUSEID3,
T_SINGLEUSEID5,
T_SINGLEUSEID7,
T_SINGLEUSEID9,
T_SINGLEUSEID10,
T_SINGLEUSEID12,
T_SINGLEUSEID13,
T_SINGLEUSEID14,
.....
....
And now only NULL car... :unamused_face:
No issue on the generated code
Generate Code
Generate
Wrote generated/gui_generated/include/gui_generated/scr_main_screen/Scr_MainViewBase.hpp
Wrote generated/gui_generated/src/scr_main_screen/Scr_MainViewBase.cpp
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Generating generated/texts/include/texts/TextKeysAndLanguages.hpp
Generating generated/texts/src/TypedTextDatabase.cpp
Generating generated/texts/src/Texts.cpp
Generating generated/texts/src/LanguageGb.cpp
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project --project-file=../GRA_10.ioc --platform=m4
Done
Done
and the result is
............................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................
2020-11-16 9:19 PM
Hello,
Could you provide the exact steps you did in order for us to reproduce and fix the issue if necessary ?
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.