2019-05-04 7:59 AM
Not really a question. I have attached a little test project for the STM32F476-Disco board using the newest ST tools. There are still problems and changes need to be made to the project. The Simulator and Build Code buttons do not work in the designer. The TouchGFX command line tool must be used for building the objects and the simulator. The simulator.exe file is located in the build folder within the TouchGFX folder. Before loading it into the target the code must be build with STM32CubeIDE.
2019-05-07 12:21 AM
Hi @hansd56,
Thanks for the feedback, that's really helpful. I'll pass it on.
/Martin
2019-05-07 12:26 AM
Just to be clear, what do you mean by "Do not work" - They're disabled or nothing happens or something else? I downloaded your project and the buttons are present here but i'm getting some post-generate error when pressing either button - Just to verify that's also what you're seeing.
Thanks!
2019-05-07 12:49 AM
2019-05-07 12:54 AM
That's great, thanks. I will pass this on.
/Martin
2019-05-07 1:25 AM
So i've figured out at least one issue - After code has been generated we call a post-generate command to update a particular project file (e.g. IAR, KEIL). But since CubeIDE is brand new, the existing command to update projects fails.
If you replace the "post generate" command in the .touchgfx file with "echo post generate" (it will complain if nothing is set), you will be able to run your simulator in the touchgfx designer at least.
2019-05-07 1:29 AM
This means that for now you have to update your CubeIDE project manually with new files (generated or otherwise).
The last problem with compiling from CubeIDE is that it's referencing libtouchgfx in a wrong way.
Go to C/C++ General -> Paths and Symbols -> Library Paths and change the entry to "/TouchGFX_Simulator/Middlewares/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc" - The linker is simply looking in the wrong spot.
2019-05-07 1:30 AM
arm-none-eabi-size TouchGFX_Simulator.elf
arm-none-eabi-objdump -h -S TouchGFX_Simulator.elf > "TouchGFX_Simulator.list"
text data bss dec hex filename
304782 252 44196 349230 5542e TouchGFX_Simulator.elf
Finished building: default.size.stdout
Finished building: TouchGFX_Simulator.list
10:27:15 Build Finished. 0 errors, 0 warnings. (took 12s.369ms)
2019-05-07 1:30 AM
So one issue i will raise is the post-generate script not being able to understand the CubeIDE format - But it's possible to update this manually for now.
2019-05-07 1:43 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.