2024-02-01 10:06 AM
Hi All
I have gone through the Touch GFX project renaming that is on YouTube. I've done this many times on the stm324f29I-DISCO and never had an issue. When using the STM32F469I I am unable to load images correctly to the GUI without them being distorted and pixelated.
Has anyone else come across this or am i doing something wrong with the project renaming? I know the board is fone becuase i have a project set up without the renaming done and it loads images fine every time.
Kind regards
Mark
2024-02-06 2:43 AM
Hello @MBode.2 ,
I'm a bit unsure about the problem that you are talking about. When you rename the project, do the pictures fail to appear correctly in TouchGFX Designer? Or do they appear distorted when you run the project on your board?
Have you tried deleting the build, config, and generated folders after renaming, and regenerating again?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.