2022-02-08 11:03 PM
MCU: STM32H7B3IIT6 Custom Board
GUI: TouchGFX Version: 4.18.1
IDE: STM32CubeIDE Version: 1.8.0
CPU Clock: 280MHz
Peripherals & Timers Clock: 140MHz
I created a new project, but there is a delay in screen interactions. I summarized the situation in the video below. Anyone have an idea about this? Why could it be.
2022-02-09 2:04 AM
Hi Freedom_Neo,
Could you give more information about your configuration please ?
I'm suspecting something like HAL_Delay() functions which might be called in your code. Is there anything like this ?
You can also verify if your clock frequency is "normal" that is to say, if 1 sec in real is 1 sec for your board. For this, I can suggest you to try to add an image that moves from a point A to a point B in 1 second for example with a "MoveAnimator" mixin (https://support.touchgfx.com/4.18/docs/development/ui-development/touchgfx-engine-features/mixins), and see if the animation is done in 1 sec, or more.
Thanks,
/Osman
2022-02-09 3:37 AM
No, I dont use HAL_Delay() functions.
Dont have time problem, I see 1 second
2022-02-10 1:55 AM
Hi Freedom_Neo,
Have you tried debugging this with break points ? Do you store your resources in an external RAM ? if it's the case, the connection between your board and your RAM might be insufficient.
/Osman
2022-02-10 2:11 AM
Segger will help you in creating widgets
In HalCube pack you have examples for all peripherials of stm32 Discovery. There ale also datasheets for discovery board, stm32, segger, and everything You need. Check out these files !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.