2023-03-16 9:45 PM
I noticed that the "video_SampleVideo2_216x216_bin_start" variable is not declared in the TouchGFX Designer-generated video playback example. Instead, it is being used in the "VideoDatabase.hpp" file as 'extern const uint8_t video_SampleVideo2_216x216_bin_start[];'. I'm curious where this variable is defined.
If possible, could you please provide a detailed explanation of where and how this variable is defined?
2023-03-16 11:40 PM
Hi,
You can find more information on video files in a TouchGFX project in this article. Basically "video_SampleVideo2_216x216_bin_start" is just a symbolic information of what was generated by the TouchGFX video converter tool which is integrated in the build tool-chain. Don't know the details of the video converter itself though sorry :grinning_face_with_sweat: nor know if we can share much about it. I'll ask.
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.