2024-03-01 7:09 PM - edited 2024-03-01 7:19 PM
Seems like there is still some problem with counting dots in file paths. However, 23.1 places all the rest of files at correct locations, unlike previous versions, which is definite progress!
See the attached screenshot.
Thanks
Solved! Go to Solution.
2024-03-14 7:11 AM
Hello @bear2023R ,
The structure of your files seems different from what you are supposed to have, why is your TouchGFX folder is at the same level as EWARM?
When I tried, I get this:
Regards,
2024-03-05 5:27 AM
Hello @bear2023R ,
I will report this issue and get back to you.
Regards,
2024-03-05 4:57 PM - edited 2024-03-05 4:57 PM
Thanks Louis
Hopefully we'll see a fix sometime soon, should be easy to fix. Meanwhile wrote and use small utility, that fixes incorrect relative paths in updated by TouchGFX Designer project file at wrong location.
Much more annoying situation that CubeMX doesn't allow to select TheadX as OS to use with TouchGFX - and only for TrustZone enabled project (see my other post from few days ago).
This also makes it necessary to do some unnecessary work of shuffling files around manually, in order to keep replacing incorrectly generated by both CuebMX and TouchGFX files for TrustZone project with those, correct ones, which were generated for non-TrustZone project.
Again, it seems like quite a simple fix required. As both generators work well for non-Trustzone project and it looks like just ThreadX option has to be enabled properly in drop-down list of OSs for TouchGFX in CubeMX... Or something like that.
A reasonably timed fix will be greatly appreciated!
Regards
2024-03-14 7:11 AM
Hello @bear2023R ,
The structure of your files seems different from what you are supposed to have, why is your TouchGFX folder is at the same level as EWARM?
When I tried, I get this:
Regards,
2024-03-26 11:13 AM - last edited on 2024-03-27 12:54 AM by LouisB
HI Louis
indeed, I have 2 TouchGFX folders: one as shown on your tree and one extra, - one level above. Probably my colleague moved it at wrong location when was copying from ThreadX-enabled project. Thanks for noting!
Best regards
2024-04-02 12:33 AM
Hello @bear2023R ,
You are welcomed, don't hesitate if you have another question.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.