2017-05-31 9:23 AM
Hello!
I am a beginner using the the NUCLEO-F746ZG to drive a 4.3' Newhaven TFT display that has a capacitive touch panel controller.
The parts are shown below:
https://www.digikey.com/product-detail/en/stmicroelectronics/NUCLEO-F746ZG/497-16282-ND/5806779
https://www.digikey.com/products/en?keywords=NHD-4.3-480272EF-ATXL%23-CTP
I was wondering if there is an example test code to see if the connections I made between the display and the nucleo are correct? I made my connections based on pins that can use the LTDC interface as an alternate function.
More info: I wish to pull images from an SD card. Certain pictures will be displayed depending on where the the user presses on the screen.
Thank you for the help!
#tft-lcd #stm32f7 #stm32 #lcd #touchSolved! Go to Solution.
2017-06-02 10:45 AM
You will need too many contact connections between the display - RGB.
F746ZG has support for DSI display contacts.The display price of NHD-4.3-480272EF-ATXL # -CTP-ND is too high. It makes sense to look for displays among cell phones, for example Explay Alto.Own design of the printed circuit board - will look better than the design on the adapters, and cheaper.
2017-06-02 4:42 PM
The DSI may have fewer wires, but the 469 also has a DSi display, and the 469 software did not come up and fly for me, like the 746g-Disco did. A few wires is not a big deal. Chasing software from a third party that does not behave can make for a lot more expense than a few wires. The less expensive display is an issue, but there are other suppliers as well. Test what works for you.
2017-06-13 10:48 PM
Hey thanks for the suggesting the tool Atollic!
Firstly, I apologize for the late response. I was forced to switch projects but I am on this case again! So right now I have wired all my connections according to the LDTC interface provided on the Nucleo. So on the Atollic, I'm guessing the only things I have to change are the LCD enable pin and the GPIO setup on the BSP_LCD_intialize function?
Right now I am using the STM32F746G_Discovery_template provided.
2017-06-13 11:09 PM
I never tried a nucleo driving the lcd, but I am using the Atollic framework to drive a 746g-disco, and it works fine. I do enable and disable the display with one pin, and don't have to rewrite it.
Sent from my Samsung device
2017-06-13 11:11 PM
Presumably the i/o setup should be done by cubemx, and you just have to drag in the bsp sources.
Sent from my Samsung device
2017-06-20 6:52 PM
Hey so I'm actually having trouble debugging my Atollic software. Does pressing the 'Debug' Icon automatically upload the firmware?
2017-06-20 7:55 PM
I believe so - I can check that in the morning. I have no stm testbed at home.Dan
Sent from my Samsung device
2017-06-21 11:14 AM
Yes, the debug under Run downloads the logic.
Dan
________________ Attachments : image001.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy0J&d=%2Fa%2F0X0000000b9v%2FYFFlUzI5na0iHZ3BtwOnFSj73ehKET2VSoH3CFMDYm8&asPdf=false2017-06-21 11:30 AM
Here is the same screen in Raisonance – cleaner and more usable in my books.
Highlighted icon above Start Debug Session is the poke point to make the download session happen.
Had a user running ST-Link yesterday to download a field update to the product we sold them recently.
Dan
________________ Attachments : image001.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyb2&d=%2Fa%2F0X0000000b9t%2F0ZuazPfkauS8bPM0MpPBv0gatKd1JVF4XSnwHcg2Z64&asPdf=false2017-06-27 11:06 AM
Hello all,
Just wanted to let you know that I have verified the connections using atollic as described by Dan. I just had trouble changing a few things, such as configurations in some C files, but eventually after changing them I was able to display a picture. Thank you all for the responses!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.