2021-04-19 6:34 AM
I have a STM32H747I-DISCO board and I'd like to test the TouchGFX on Windows10. I designed a simple application with 2 screens and 2 buttons, and it runs ok on the simulator. But I get an error when exporting to the target.
Here is the complete error message:
Run Target
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Converting images
Reading ./application.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj && touchgfx update_project --project-file=../EWARM/TouchGFX.ewp
Done
Compile
make -f ../gcc/Makefile -j8
Converting images
Reading TouchGFX/application.config
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
Done
Flash
make -f ../gcc/Makefile -j8 flash
Converting images
Reading TouchGFX/application.config
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0
-------------------------------------------------------------------
ST-LINK SN : 003400373037510339373532
ST-LINK FW : V3J7M2
Board : STM32H747I-DISCO
Voltage : 3.22V
Error: No STM32 target found!
2nd connect tentative with a lower frequency (8MHz)
ST-LINK SN : 003400373037510339373532
ST-LINK FW : V3J7M2
Board : STM32H747I-DISCO
Voltage : 3.22V
Error: No STM32 target found!
make[1]: *** [_extflash_] Error 1
c:/TouchGFXProjects/DemoApp/gcc/include/flash_sections_int_ext.mk:2: recipe for target '_extflash_' failed
../gcc/Makefile:50: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
FailedCan anyone help?
Thanks a lot!
2021-04-23 2:17 AM
Well good to hear that you are able to work with one now ^^
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.