2020-04-22 12:33 AM
Dear all,
We often receive new ideas for improving our STM32 hardware and software, and these ideas are often scattered around the community in different posts. This is making it difficult to be aware of all and to consolidate each single idea and get community feedback. To improve they way of providing new ideas for a new widget, new feature, improved usability, etc. to TouchGFX, we have created an “IDEA�? forum, where these can be posted and everyone can comment and upvote/downvote.
Before we release this new feature we need some of you to help us test it and provide feedback for improvements. If you are find this interesting, please let us know.
Best regards
Soren Mikkelsen
2020-04-22 1:51 AM
Yes, very much!
I tried to start a similar thread a while back but it never really caught on.
this concept is similar across a lot of programs/platforms and I know that for example Autodesk does a similar thing with fusion360 feature requests
Count me in!
2020-04-22 1:53 AM
Great @HP
I will write you an email with further details.
2020-04-22 3:58 AM
Hello,
@Soren Myllerup MIKKELSEN (ST Employee)
Thanks for the Topic ..
I am interested if more TouchGFX Demo(s) are combined with USB Mass Storage / SDCard / LEDs /Hardware Switches /UART /CAN/ Ethernet/ WiFi
So, Actual deployment and usability can be easy while modifying or referencing that demo(s) in our Projects/Products.
--
Karan
2020-04-22 1:31 PM
I am interested and would help to test
2020-04-23 12:31 AM
Hello Karan,
This is exactly the kind of ideas we need from the community. When IDEAS gets online, please post your ideas there. thanks.
Best regards
Soren
2020-04-23 12:32 AM
Great Dr.Electron!
I will send you an email with further information.
Br
Soren
2020-04-23 2:09 AM
@Soren Myllerup MIKKELSEN (ST Employee)
Yaa... Sure..
What kind of test you want as feedback from my Side ?
I have STM32F746G-DISCO board . I have experience of GUI programming from other Semiconductor companies ...
TouchGFX and C++ is quite new for me ..
--
Karan
2020-04-23 3:16 AM
did you write me a mail @Soren Myllerup MIKKELSEN ? I haven't seen anything yet :)
2020-04-23 10:59 AM
Great :) This is the way, also other "departments" of st should handle the stuff ;) But as usual: the TouchGFX team doesn´t disappoint me :) If you´re interested: I have several F746 and F769 discovery boards for tests lying around here ;)
The 1st Ideas, when it comes to a "wishlist" would be:
a) a simple "link mechanism" to freeRTOS semaphores and queues (not really necessary, as long, as the interactions with external code can handle this very well, but it could be helpful, to have tGFX "keeping an eye" on them. This would lead to being expandable even with a FSM inside tGFX)
b) a keyboard widget (usable as standard keyboard, like in the examples, and as a numpad) in the designer. Easy to configure and to skin ;)
/Charly
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.