2025-04-06 12:27 PM - edited 2025-04-06 12:34 PM
Hey,
I have a confusing error, i have a Riverdi 7" TFT Panel (https://download.riverdi.com/RVT70HSTNWC00-B/DS_RVT70HSTNWC00-B_Rev.1.2.pdf)
Actually my LTDC Init is this:
static void MX_LTDC_Init(void)
{
/* USER CODE BEGIN LTDC_Init 0 */
/* USER CODE END LTDC_Init 0 */
LTDC_LayerCfgTypeDef pLayerCfg = {0};
/* USER CODE BEGIN LTDC_Init 1 */
/* USER CODE END LTDC_Init 1 */
hltdc.Instance = LTDC;
hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
hltdc.Init.HorizontalSync = 0;
hltdc.Init.VerticalSync = 0;
hltdc.Init.AccumulatedHBP = 160;
hltdc.Init.AccumulatedVBP = 23;
hltdc.Init.AccumulatedActiveW = 1184;
hltdc.Init.AccumulatedActiveH = 623;
hltdc.Init.TotalWidth = 1344;
hltdc.Init.TotalHeigh = 635;
hltdc.Init.Backcolor.Blue = 0;
hltdc.Init.Backcolor.Green = 0;
hltdc.Init.Backcolor.Red = 0;
if (HAL_LTDC_Init(&hltdc) != HAL_OK)
{
Error_Handler();
}
pLayerCfg.WindowX0 = 0;
pLayerCfg.WindowX1 = 1024;
pLayerCfg.WindowY0 = 0;
pLayerCfg.WindowY1 = 600;
pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB888;
pLayerCfg.Alpha = 255;
pLayerCfg.Alpha0 = 255;
pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
pLayerCfg.FBStartAdress = 0xC0000000;
pLayerCfg.ImageWidth = 1024;
pLayerCfg.ImageHeight = 600;
pLayerCfg.Backcolor.Blue = 255;
pLayerCfg.Backcolor.Green = 0;
pLayerCfg.Backcolor.Red = 0;
if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN LTDC_Init 2 */
/* USER CODE END LTDC_Init 2 */
}the Layer0 background is set to blue, if my WindowsX1 = 1024, my background shows no blue screen, but only gray..
if i decrease WindowX1 to 500, then my screen is half blue, if i change WindowsX1 to 0 then my Screen are complete blue..
whats wrong? my LCD is in 18-Bit mode (RGB666) and V/HSync and the DCLK of the display is 50 MHZ, Pixel Format is set to RGB888.
my external sdram works fine, here is the test result:
-------------------- SDRAM 16 bit access -------------------
Write 16-bit data , size: 32 MB, elapsed time: 825 ms, write speed: 38.79 MB/s
Read 16-bit data, size: 32 MB, elapsed time: 3161 ms, read speed: 10.12 MB/s
-------------------- 16 Bit data validation -------------------
SDRAM 16-bit data validation pass!
Solved! Go to Solution.
2025-04-09 10:29 PM
Hello Gaetan,
Thank you, i contacted the guys at Riverdi, and they help me.
The Settings for my TFT was a little bit wrong, after the changed, touchGFX worked :)
Regards,
Daniel
2025-04-09 6:53 AM
Hello @Sany ,
It looks like expected behavior.
Meaning that the blue background is there is nothing happens.
When you have X1 at 1024, the transfer happens so you transfer the framebuffer and when you reduce X1 to 0, nothing gets transferred so only the default blue background is showing.
Have you enabled TouchGFX? What is the content of your framebuffer?
Can you change some colors and see how your display behaves?
Regards,
2025-04-09 10:29 PM
Hello Gaetan,
Thank you, i contacted the guys at Riverdi, and they help me.
The Settings for my TFT was a little bit wrong, after the changed, touchGFX worked :)
Regards,
Daniel
2025-04-10 12:39 AM - edited 2025-04-10 12:40 AM
Please share Reverdi settings before accepting the solution.
This to ensure that someone else could find the solution if he fall into the same issue.
Thank you.
2025-04-10 2:18 AM
Hello @Sany ,
I am glad to hear that!
Can you share what was the issue?
Regards,
2025-10-03 9:53 AM
Dear Sir I have dev a pcb based on stm32h743ii serie and i have the same carracteristique 7 inch display .
Do reverdi provide rgb888 24 bit driver or you have write it alone ?
yours faithfully
Khales
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.