2017-11-29 9:15 AM
Hi.
I want to make an analog monitor with tvp5150am1 and I have a few questions.
Can I connect TVP5150AM1 to DMA2D?I found &sharpdefine DMA2D_INPUT_YCBCR in the code, but in CubeMX no, what does that mean?Can I do without an outside SDRAM? (Display 800x480).Any advice?#dma2d #display #camera #stm32h72017-11-29 1:17 PM
You want to monitor the 8Bit YCbCr signal output from the TI device, right?
(because the TVP5150AM1 has analog inputs)
The DMA2D is a Controller to manipulate images, like filling, copying or blending parts of an image in RAM.
It does have just one input pin: 32-bit AXI bus clock
Read the output and HSYNC/VSYNC with ordinary gpio pins, but you have to drive the YOUT[6:0] pins externally or pull down with a 10k resistor.
2017-11-30 12:57 AM
I wanted to do this: TVP5150AM1 -> DCMI -> DMA2D YCBCR to RGB -> LTDC -> 18bit display
2017-11-30 1:51 AM
Oh ya, I forgot the camera interface. DCMI offers everything you will need.
Pixel clock x1 input, HSYNC and VSYNC. Save the data with DMA in memory,
do the conversion and feed the LTDC. In CubeMX you can select the transfer
mode 'Memory to Memory with 'Pixel Format Conversion''.
Which chip do you want to use on your board?
2017-12-04 12:20 AM
STM32H753XIH6
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.