cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f746IG interfacing with ADV7180 camera driver

Uc.2361
Associate II

I have taken a sample camera code of stm32f756 eval board in which the camera driver ic was S5K5CAG.

and interfaced the dcmi peripheral and i2c configuration peripheral but i am unable to display camera output on the LCD display. I am using ADV7180 camera driver IC and I dont have perfect driver code for that IC.

The ADV7180 ALSB pin is pulled up so the i2c address i used is 0x42.

Can anyone please help me out, I am struck with this from 2 days. I am able to display text on LCD as far as now.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Uc.2361
Associate II

Hello,

Can any one help me to figure out the solution for the above issue.

Thanks

I am able to communicate with the adv7180 device for writing and reading the registers but the camera visuals are not able to display on the LCD.

What are scenarios need to be taken care.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.