2021-12-06 7:43 AM
In GUI_Conf.c, allocated the memory size for GUI.And in LCD_Conf.c file, declared the size of display ,configured the flexcolor driver for ILI9341 controller.And aslo implemented the read and write function by using SPI. In order to resolve the Hardfaul handler(), I have changed the Stack and Heap size and also change the memory allocation for GUI. Is there any configuratio n need to be done?
2021-12-06 9:25 AM
Hello @Kanna ,
Please share the source code to check more the configuration and the behavior.
Did you called the GUI_Init() function and enabled the CRC module ?
GUI_Init() should be used to initialize the STemWin internal data structures and variables. And performs the initialization of the display by calling the function LCD_X_Config().
I advise you to have a look at the AN4323 Application note Getting started with STemWin Library.
Imen
2021-12-06 9:30 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.