2016-03-09 5:24 AM
Hi all,
I have problem with displaying any data at WF57STIACDNN0 TFT display. This is a TFT display with ST7511U driver. In my SW driver I successfully pass the display initialization procedure - I see some randomize pixels set, but I am NOT able to display any data by write RAM command - 0x2C (ST75_WRAM). First my goal is to clear whole display and set each pixel on the screen. For communication I am using 4 line (A0 + SPI). In the past I only wrote some drivers for easy ALPHA display so I have no any knowledge about graphic display. Below I will put by initialize function and function where I would like to clear whole display area. staticvoid
display_init(){
CS_ENABLE
;spi_write_command(
ST75_SWRESET
);spi_write_data(
0xa5
);//Power
Control
spi_write_command(
ST75_PWRCTL
);spi_write_data(
0x8f
);//booster
setting
=
''10''
=
-2
??
spi_write_data(
0x04
);//SAMPSet
=
''100''
??
spi_write_data(
0xa5
);//WARNING
in
spec
is
0x0a5
??
spi_write_data(
0xa5
);//Electronic
Volume
Set
1
spi_write_command(
ST75_EVSET1
);spi_write_data(
0x36
);//VCOM
??
spi_write_data(
0x0b
);//VGHREG
??
spi_write_data(
0x0b
);//VGLREG
??
spi_write_data(
0xa5
);//Display
area
spi_write_command(
0x31
);spi_write_data(
0x00
);spi_write_data(
0xEF
);//0
-
239
=
240
spi_write_data(
0x02
);spi_write_data(
0x7F
);//Display
Set
2:
Set
source
and
gate
ON/OFF
timing
spi_write_command(
ST75_DISSET2
);spi_write_data(
0x07
);spi_write_data(
0x2c
);spi_write_data(
0x09
);spi_write_data(
0x2a
);//Electronic
Volume
Set
2
spi_write_command(
ST75_EVSET2
);spi_write_data(
0x09
);//GVDD[4:0]
??
spi_write_data(
0x17
);//GVCL[4:0]
??
spi_write_data(
0xa5
);//
spi_write_data(
0xa5
);//
//Gamma
Set
4bpp
Positive
1
spi_write_command(
ST75_GAMSET4P1
);spi_write_data(
0x00
);spi_write_data(
0x16
);spi_write_data(
0x1B
);spi_write_data(
0x1C
);spi_write_command(
ST75_GAMSET4P2
);spi_write_data(
0x1E
);spi_write_data(
0x1F
);spi_write_data(
0x20
);spi_write_data(
0x21
);spi_write_command(
ST75_GAMSET4P3
);spi_write_data(
0x23
);spi_write_data(
0x24
);spi_write_data(
0x26
);spi_write_data(
0x28
);spi_write_command(
ST75_GAMSET4P4
);spi_write_data(
0x2B
);spi_write_data(
0x2F
);spi_write_data(
0x34
);spi_write_data(
0x3f
);//Gamma
Set
4bpp
Negative
1
spi_write_command(
ST75_GAMSET4N1
);spi_write_data(
0x00
);spi_write_data(
0x16
);spi_write_data(
0x1B
);spi_write_data(
0x1C
);spi_write_command(
ST75_GAMSET4N2
);spi_write_data(
0x1E
);spi_write_data(
0x1F
);spi_write_data(
0x20
);spi_write_data(
0x21
);spi_write_command(
ST75_GAMSET4N3
);spi_write_data(
0x23
);spi_write_data(
0x24
);spi_write_data(
0x26
);spi_write_data(
0x28
);spi_write_command(
ST75_GAMSET4N4
);spi_write_data(
0x2B
);spi_write_data(
0x2F
);spi_write_data(
0x34
);spi_write_data(
0x3F
);//Sleep
Out
spi_write_command(
ST75_SLPOUT
);spi_write_data(
0xA5
);&sharpif
1
/*
is
set
to
ZERO
by
default
!!!*/
//Memory
Address
Control:
Set
about
display
data
RAM.
/*
Select
address
incremental
direction:
*
MV
-
0
(Incremental
column
addr.)
*
Display
data
RAM
page
address:
*
MY
-
0
(Normal)
*
Display
data
RAM
column
address
*
MX
-
0
(Normal)
*/
spi_write_command(
ST75_MADCTL
);//sleep_ms(2);
//sleep
is
required
by
specyficatrion
ST7511U
spi_write_data(
0x00
);//in
spec
is
set
to
0x01
[F57STIACDNN0]
spi_write_data(
0xA5
);spi_write_data(
0xA5
);spi_write_data(
0xA5
);&sharpendif
//BPP
Select:
Set
data
format
(bit
per
pixel)
BPP
spi_write_command(
ST75_BPPSEL
);spi_write_data(
0x00
);//
1bpp,
(2
gray
scale)
1
bit
per
pixel
spi_write_data(
0xA5
);spi_write_data(
0xA5
);spi_write_data(
0xA5
);spi_write_command(
0x25
);//page
address
set
spi_write_data(
0x00
);//start
0
spi_write_data(
0x29
);//end
41
spi_write_data(
0x00
);spi_write_data(
0xa5
);spi_write_command(
0x26
);//Collumn
address
set
spi_write_data(
0x00
);//start
0
spi_write_data(
0x00
);//
spi_write_data(
0x01
);//end
479
spi_write_data(
0xdf
);//Display
on
spi_write_command(
ST75_DISON
);spi_write_data(
0xA5
);asm
(''NOP''
);CS_DISABLE
;}
And hear the function when I would like to clear whole display area:void
ST75_display_clr(){
UInt16_t
i,j;//640/320
ST75_set_window(
0
,639
,0
,320
);spi_write_command(
ST75_WRRAM
);for
(i=0
; i<30
; i++) {for
(j =0
; j<639
; j++) {spi_write_data(
0x00
);}
}
}//640/320
static
void
ST75_set_window(UInt16_t
s_x,UInt16_t
e_x,UInt16_t
s_y,UInt16_t
e_y){
//x,
max
=
640
//CSA:
Set
column
START
addres
spi_write_command(
ST75_CASET
);spi_write_data(s_x >>
8
);spi_write_data((
UInt8_t
)s_x);//max
=
//CEA:
Set
column
END
address
spi_write_data(e_x >>
8
);//end
479
spi_write_data((
UInt8_t
)e_x);//y,
max
=
160
spi_write_command(
ST75_PASET
);//PSA:
Set
page
START
address
spi_write_data(s_y);
//x
max
=
//PEA:
Set
page
END
address
spi_write_data(e_y);
//DEFAULT
//FrmA:
Set
frame
address
-
00
spi_write_data(
0x00
);//DEFAULT
spi_write_data(
0xA5
);}
Br, ToR #tf #winstar #display #lcd #stm32We’re moving the ST Community to a new platform to give you a better and more reliable community experience.