2023-04-27 10:44 PM
Hi, as per datasheet of STM32F412VG all IO's are compliant (page 124) to CMOS & TTL, it's OK for input signal, but while configuring pin as output, how we will come to know logic level for the same, as VOH (min) is 2.4 for TTL & for CMOS it is (VDD-0.4) for 3.3 operating it will be 2.9V
i am interfacing device, where min. VIH (min) requirement is 2.48V, if controller pin is with TTL, it may create an issue
2023-04-27 10:49 PM
You cannot select between CMOS or TTL.
It's either input, open drain, or an "active" push-pull output, which is the one you need.
If you don't have super high load or transmission losses, the STM's high level will be very close to its supply voltage.
What is actually the other device, and what is its supply voltage?
2023-04-27 11:35 PM
Hi , it is an LCD,
for controller VOH(min)
in CMOS (VDD-0.4), i.e. for any operating voltage higher than 2.9V it is greater than required level of 2.48V
but in TTL it is fixed 2.4V for any operating voltage, higher than 2.4V
my LCD operates on 3.1VDC, it's required VIL(max) is 0.62V & VIH(min) is 2.48V
so to full fill minimum VIH level, i need to ensure controller o/p logic levels remains as per CMOS
2023-04-28 3:35 AM
Interesting that the display runs on 3.1 V (I have zero experience with displays).
So you can definitely use the STM32 GPIOs, but for IO protection you should use some serial resistors, depending on line impedance / frequency, I would start with 49R9 or 47R.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.