2019-03-31 6:12 PM
I am using the STemWin BASIC_HellowWorld Application.
I modified the source code to look like this:
void MainTask(void) {
char counterstring[128];
int counter = 1;
GUI_Clear();
GUI_SetFont(&GUI_Font32_1);
while(1)
{
HAL_Delay(1);
sprintf(counterstring,"Time %d",counter++);
GUI_DispStringAt(counterstring, 0, 0);
}
}It prints out 13 times. Then emWin stops updating the display, even though the debugger shows the process is still running and the counter is incrementing, If I change the HAL delay to 2, it prints 9 times; if I change it to 3, it prints 6 times. If I change it to 0 it prints 139 times.
It looks like emWin just stops working after ~20 ms. Any clues, suggestions, or hints?
EDIT: I am using the STM32F769-Discovery kit with a 30-day evaluation version of IAR.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.