2014-03-04 2:02 PM
Hello I'm running the RTos Demo for STM324xG eval and have a lot of trouble with Interrupts. For example transfer via Uart is broken. Pieces are missing. I force it in a loop when transfer starts, thats works but isn't the sense of running a RTos system. Could someone says something about Priority settings used by STemWin? Or has someone a working Uart sample to receive and send witch is tested with STemWin and FreeRtos?
Thanks in advance Joerg #stemwin-freertos-priority2014-03-04 6:35 PM
Not sure why the USART would fail, but you don't have to switch tasks, I'd opt to buffer the data.
2014-03-04 11:04 PM
Hello,
The are buffered. Not sure thats ok as it done. The lib is not build by me. Now I do so:static void Background_Task(void * pvParameters)
{ /* Initilize the BSP layer */ BSP_Init(); /* Activate the use of memory device feature */ WM_SetCreateFlags(WM_CF_MEMDEV); /* Init the STemWin GUI Library */ GUI_Init(); UB_Uart_Init(); char buf[RX_BUF_SIZE]; // puffer fuer Datenempfang UART_RXSTATUS_t check; /* Run the background task */ while (1) { /* toggle LED1..4 each 100ms */ // STM_EVAL_LEDToggle(LED1); // check ob Daten an UART2 empfangen werden check=UB_Uart_ReceiveString(COM3,buf); if(check==RX_READY) { // wenn Daten empfangen wurden // als Echo wieder zurücksenden UB_Uart_SendString(COM2,buf,LFCR); }GUI_Delay(1);
} } Thats works butIf I do it without the while loop it looks like :
mailto:28F5C9D0040000C9@0000 mailto:28BB90BF040000C3@6875 DHTOK@49 mailto:28F5C9D0040000C9@0000 @6875 mailto:28F5C9D0040000C9@0000 mailto:28F5C9D0040000C9@0000 @49 mailto:28F5C9D0040000C9@0000 mailto:00C3@6875 9 mailto:28F5C9D0040000C9@0000 mailto:28BB90BF040000C3@6875 DHTOK@49
________________
Attachments : stm32_ub_uart.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzTF&d=%2Fa%2F0X0000000bMQ%2FiZziX.ta5Viga3XAnDWXBivDLIXLi3w4YpVa.jlOEjo&asPdf=falsestm32_ub_uart.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzTi&d=%2Fa%2F0X0000000bMO%2FosaZ_JO1jU28uKxYCZOGY53VQ5HKxXFs2gjzZzabRec&asPdf=false
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.