2019-12-04 2:03 PM
I am developping a vu-meter with STM32F476G-DISCO + TouchGFX 4.12.3.
The line is plotted but there are some strange effect in some positions probably a bug of the line function or graphic environment.
Also in the simulation the same effect.
here some better result with the optional code
I can share the complete project if necessary for the debug.
void Screen2View::handleTickEvent()
{
if (count < 2)
{
count++;
return;
}
// optional code to get a better result
//left.setLineWidth(0);
//left.invalidate();
count = 0;
if (value < 1024) value += 10;
else value = 0;
float value1 = (value * 68 / 1022) + 56;
plot((float)value1, 179.0, 350.0, 128.0, 313.0);
left.setLineWidth(2);
left.invalidate();
}
void Screen2View::plot(float level, float x0, float y0, float ymax, float r)
{
#define C 3.141592/180.0
char buf[30];
float s, c, r2, x1, x2, y1, y2;
s = sin(level * C);
c = cos(level * C);
x1 = x0 + (r * c);
y1 = y0 - (r * s);
r2 = (y0 - ymax) / s;
y2 = ymax;
x2 = x0 + (r2 * c);
#ifdef SIMULATOR
sprintf(buf, "line %d,%d,%d,%d", (int)x1, (int)y1, (int)x2, (int)y2);
touchgfx_printf("%s \n", buf);
#endif
left.setLine((int)x1, (int)y1, (int)x2, (int)y2);
}
2019-12-05 1:27 AM
I don't know why but this solve the problem
void Screen2View::handleTickEvent()
{
left.invalidate();
if (value < 1024) value += 10;
else value = 0;
float value1 = (value * 68 / 1022) + 56;
plot((float)value1, 179.0, 350.0, 128.0, 313.0);
left.invalidate();
}
void Screen2View::plot(float level, float x0, float y0, float ymax, float r)
{
#define C 3.141592/180.0
char buf[30];
float s, c, r2, x1, x2, y1, y2;
s = sin(level * C);
c = cos(level * C);
x1 = x0 + (r * c);
y1 = y0 - (r * s);
r2 = (y0 - ymax) / s;
y2 = ymax;
x2 = x0 + (r2 * c);
left.setLine((int)x1, (int)y1, (int)x2, (int)y2);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.