2024-09-09 5:59 AM - last edited on 2024-09-09 6:13 AM by mƎALLEm
will this code work?
#include <gui/screen3_screen/Screen3View.hpp>
//#include <math.h>
#define PI 3.1415926
// Declare the DAC handle (assuming it's defined in another file)
extern DAC_HandleTypeDef hdac1;
static bool generateSineWave = false; // Flag to control sine wave generation
Screen3View::Screen3View()
: end1(172), end2(141), max1(480), max2(200) // Initialize sine wave parameters
{
}
void Screen3View::setupScreen()
{
Screen3ViewBase::setupScreen();
}
void Screen3View::tearDownScreen()
{
Screen3ViewBase::tearDownScreen();
}
void Screen3View::get_sineval()
{
// Generate sine wave values for both DAC channels
for (int i = 0; i < end1; i++)
{
value1[i] = ((sin(i * 2 * PI / end1) + 1) * (max1 / 2)); // Sine values for Channel 1
}
for (int i = 0; i < end2; i++)
{
value2[i] = ((sin(i * 2 * PI / end2) + 1) * (max2 / 2)); // Sine values for Channel 2
}
}
void Screen3View::buttonClicked()
{
generateSineWave = !generateSineWave; // Toggle the sine wave generation on/off
if (generateSineWave)
{
get_sineval(); // Generate the sine wave values
// Start the DAC for both channels
HAL_DAC_Start(&hdac1, DAC_CHANNEL_1); // Start DAC for Channel 1
HAL_DAC_Start(&hdac1, DAC_CHANNEL_2); // Start DAC for Channel 2
}
else
{
// Stop the DAC when the button is pressed again
HAL_DAC_Stop(&hdac1, DAC_CHANNEL_1);
HAL_DAC_Stop(&hdac1, DAC_CHANNEL_2);
}
}
void Screen3View::tickEvent()
{
Screen3ViewBase::tickEvent(); // Call the base class tickEvent
if (generateSineWave)
{
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, value1[time1]);
time1+=1;
if (time1>end1-1)
time1=0;
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_2, DAC_ALIGN_12B_R, value2[time2]);
time2+=1;
if (time2>end2-1)
time2=0;
}
}
Solved! Go to Solution.
2024-09-09 6:12 AM - edited 2024-09-09 6:21 AM
Hello @Sharan ,
In next time kindly use </> button to share your code. I'm editing your post then ..
Please review our recommendation in this link on how to post a thread.
@Sharan wrote:
will this code work?
Did you test it?
From my point of view, you don't have to call HAL drivers from GUI (View), you need to pass the command of DAC On/Off over GUI layers: view -> presenter -> model -> HAL
Thank you.
2024-09-09 6:12 AM - edited 2024-09-09 6:21 AM
Hello @Sharan ,
In next time kindly use </> button to share your code. I'm editing your post then ..
Please review our recommendation in this link on how to post a thread.
@Sharan wrote:
will this code work?
Did you test it?
From my point of view, you don't have to call HAL drivers from GUI (View), you need to pass the command of DAC On/Off over GUI layers: view -> presenter -> model -> HAL
Thank you.
2024-09-09 10:07 PM - edited 2024-09-10 3:45 AM
hi i tried the code it did not work
where do i have to write my code ,in presenter.cpp or model.cpp or view.cpp
2024-09-13 1:57 AM
Hello,
You need to write code in view.cpp, presenter.cpp and model.cpp according to Model-View-Presenter Design Pattern.
Watch this video.
In model you start to interact with HAL/Hardware.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.