2025-04-29 6:00 AM - edited 2025-04-29 6:00 AM
I have created a scroll list object in TouchGFX Designer. The Scroll List takes a custom container as item. I have 3 items in my scroll list
For some reason, when I call languageSelectorScrollListItems.getNumberOfDrawables(); it returns 5
Checking the member declaration I'm seeing that it is defined as an array with 5 items
2025-04-29 7:06 AM
Ok so for some reason the languageSelectorScrollListItems is set as an array of 5 elements. What I needed was instead the languageSelectorScroll.getNumberOfItems() which returns the correct numbers of items in the Scroll List.
I'll keep this post open to understand why languageSelectorScrollListItems has been set to a fixed 5
2025-05-01 1:10 AM
From what I'm understanding, the getNumberOfDrawables just returns the number of, in fact, drawables in your costume container that will be used as an item + 1.
So, if, in my costume container, I have just a text area, it will return 2.
To get the number of items in the list, the method is getNumberOfItems
Now, I still have to understand how to access the specific item (for instance, I want to access item number 3 of the scroll list) and then access the text area of that specific item. Is there a way to do that or do I need to implement code to trace the index of every item beforehand to access them?
2025-05-01 11:22 AM
Check Demo9, it uses a custom table to do the association between enum/value/bitmap in
SubeDemoInfo.hpp (yes there is a typo in their filename).
sphere_wheelBase::setAnimationEnddedCallback()
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.