2020-02-05 7:21 AM
Hi,
I have a problem with STM32CubeIDE 1.2.0 and TouchGFX 4.13.0.
I use the STM32F746G-DISCO board. First, I created a project with TouchGFX to check if the screen works. It works well !
After that, I created a project with CubeIDE. I configured the pinout manually and I was able to display an image on the board via a .h file.
When I add TouchGFX Generator in "Additional Software", it creates the TouchGFX folder. I changed the .touchgfx file but the screen still black when I launch the project on the target.
Could you help me please ?
It is very important.
Solved! Go to Solution.
2020-02-06 2:50 AM
Hi,
This solved my problem : https://community.st.com/s/question/0D50X0000C211khSQA/working-example-st32f469disco-cubeide-touchgfx-413-
Best Regards
2020-02-06 12:44 AM
Same Problem here with an STM32L4R9 Custom Board with GFXMMU enabled.
I can manually fill the Screen with a Color (DMA2D_R2M) and a picture via .h file. But TouchGFX shows nothing. RTOS is freezing and my code is all the Time in LTDC Error Interrupts ( FIFO Underrund and Transfer Error)
Some ideas?
2020-02-06 2:50 AM
Hi,
This solved my problem : https://community.st.com/s/question/0D50X0000C211khSQA/working-example-st32f469disco-cubeide-touchgfx-413-
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.