2025-03-10 7:51 PM
Hi,
as you can see in the first screenshot, in the X-CUBE-TOUCHGFX settings (TouchGFX Generator tab) the LTDC option for the Application Tick Source is not available. And at the bottom it says "LTDC in only available if enabled".
LTDC is enabled and configured (second screenshot). Does it need to be configured and/or enabled in some other ways or some other place too?
Thank you :)
Solved! Go to Solution.
2025-03-11 3:37 AM
Yes, in your first screenshot, under Display -> Interface, you have the change the value from Custom to LTDC.
2025-03-11 3:37 AM
Yes, in your first screenshot, under Display -> Interface, you have the change the value from Custom to LTDC.
2025-03-11 8:29 AM
Thank you @jchernus-fikst
but as you can see it is greyed out and cannot be selected. I was asking why and what else I would need to enable in order for it to not be greyed out so I can select it.
Thank you :)
2025-03-12 3:21 AM
Please re-read my answer.
Your question asked about Driver -> Application Tick Source. I'm suggesting you change Display -> Interface. These are two different things.
Julia
2025-03-12 9:21 AM
Sorry @jchernus-fikst long days i front of the PC, I misread your answer.
Yes, now it works.
Thank you! :)
2025-03-12 11:15 AM
Great! Happy it works, I got stuck on this too just a few weeks ago. Their instructions are not very clear.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.