2019-07-24 1:10 AM
I use a scroll list dinamic.
When i set itemSelectedCallback the itemIndex don't reach maximun element.
For example:
sl_select.setNumberOfItems(4);
sl_select.setWindowSize(4);where max number of object can be 4, param of itemSelectedCallback pass only 0 for itemIndex.
Other example is:
sl_select.setNumberOfItems(13);
sl_select.setWindowSize(5);where max number of object can be 13, max param of itemSelectedCallback pass is 9 for itemIndex.
What do it wrong?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.