2021-08-15 10:29 PM
Hi,
I am new to STM32F7508-DK. I'm running it's sample LTDC_PicturesFromSDCard, I only want to display image in the board that is present in the sd card.
But still get some error with FLASH memory. This is the error:
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down...
After this, the LCD turns white and nothing happens.
Any help is really appreciated.
2021-08-16 5:42 AM
Hello @AGaut.3 and welcome to the Community :)
Are you using the latest release of STM32CubeProgrammer ? Try select "Erasing & Programming" on the left, then do a "Full chip erase".
Please make sure also to follow this article Why my STM32 doesn't start?
If your issue is solved, please select the answe as “Best�? as this will help other users to find this response faster.
Imen
2021-08-24 9:17 PM
Yes, I'm using the latest release of STM32CubeProgrammer. And, I tried "Full chip erase" but that didn't worked for me. Any suggestions please..
2021-08-24 9:26 PM
The application should run without being connected to the debugger.
As I recall the application should put some text on the screen absent any sdcard
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.