2019-06-27 10:43 AM
I running an application on STM32F769 with EWARM that connect to Servers from the net and receiving data (with Net Thread) . Next i added all necessery files and a graphic Thread in main file to display the data on th lcd when i pressed on a button . When i run the application the lcd works and the button appear but the Net Thread blocked on the instruction ( MX_LWIP_Init();)
PS: when i comment the instruction GRAPHICS_Init(); the board connect to the Net
Solved! Go to Solution.
2019-07-01 9:22 AM
Hi @Martin KJELDSEN
The problem is that I choose TIM1 as a timebase source, this timer is used in STM32F7Instrumentation::init. I change the timebase from TIM1 to TIM6 and it work.
Thank you @Martin KJELDSEN for your assistant.
2019-06-28 1:02 AM
Hi @youssef.amimi,
I'll try to think about what's wrong here. I'm not that familar with lwip + TouchGFX, but we have a few projects here that we did a while back. The LWIP stack in CubeFW does have it's own issues, so iI'll have to get back to you, is that allright?
Best regards,
Martin
2019-06-28 6:42 AM
Hi @Martin KJELDSEN ,
Ok, thanks for your interest, I will wait for your reply and i will report any progress i have.
Best regards,
Youssef
2019-06-30 1:50 PM
Great, thanks. I'll try to give it a look tomorrow when i'm at the office,
/Martin
2019-07-01 5:29 AM
Hi Youssef,
How did you create your ethernet interface configuration? Did you copy it or get it through CubeMX? For the project we have here we the following remarks:
Besides removing the call to Graphics_init(); did you do any additional debugging? GRAPHICS_init() sets up TouchGFX with the correct HAL and DMA classes, sets the pointer to the start of the framebuffer, etc (Only initialization).
void touchgfx_init()
{
uint16_t dispWidth = 480;
uint16_t dispHeight = 272;
HAL& hal = touchgfx_generic_init<STM32F7HAL>(dma, display, tc, dispWidth, dispHeight, (uint16_t*) 0,
0, 0);
hal.setFrameBufferStartAddress((uint16_t*)frameBuf0, bitdepth, true, true);
hal.setTouchSampleRate(2);
hal.setFingerSize(1);
// By default frame rate compensation is off.
// Enable frame rate compensation to smooth out animations in case there is periodic slow frame rates.
hal.setFrameRateCompensation(false);
// This platform can handle simultaneous DMA and TFT accesses to SDRAM, so disable lock to increase performance.
hal.lockDMAToFrontPorch(false);
mcuInstr.init();
//Set MCU instrumentation and Load calculation
hal.setMCUInstrumentation(&mcuInstr);
hal.enableMCULoadCalculation(true);
}One thing you can try to verify the DMA issue is the following - Use NoDMA instead of STM32F7DMA which is the default for F7 based projects.
NoDMA dma;
STM32F746GTouchController tc;
STM32F7Instrumentation mcuInstr;
LCD16bpp display;
uint32_t cache[(250*250*3+1000)/4];
void touchgfx_init()
{
HAL& hal = touchgfx_generic_init<STM32F7HAL>(dma, display, tc, 480, 272, (uint16_t*)cache, sizeof(cache), 1);
os_inited = true;
...Does that make sense? Let me know.
/Martin
2019-07-01 6:00 AM
Hi @Martin KJELDSEN
I create my ethernet interface configuration through CubeMX and it worked alone.
I tried to do additionnal debugging and i found that the Net Thread enter in the fonction HAL_Delay(PHY_RESET_DELAY);(in fonction HAL_ETH_Init on file stm32f7xx_hal_eth.c) and never go out.
I use NoDMA instead of STM32F7DMA but steel don't work
2019-07-01 6:49 AM
PS: When i run with the net configuration alone :
in the HAL_DELAY the variable uwTick = 3(from fonction HAL_GetTick()) incriment until uwTick-tickstart > wait (wait = 256 and tickstart = 3) but when i add graphic the variable uwTick = 1271 is not incrimented (tickstart = 1271 and wait = 256), that's why it never go out.
I didn't find out why uwtick is not incrimented.
2019-07-01 9:22 AM
Hi @Martin KJELDSEN
The problem is that I choose TIM1 as a timebase source, this timer is used in STM32F7Instrumentation::init. I change the timebase from TIM1 to TIM6 and it work.
Thank you @Martin KJELDSEN for your assistant.
2019-07-01 11:51 PM
Ah, that's good news. Good job finding that.
/Martin
2019-07-02 1:18 AM
Thank you @Martin KJELDSEN
Youssef
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.