2023-01-26 6:40 AM
Hello everyone,
I am designing a datalogger with a touch screen and I am undecided in the selection of the method to control the screen, do you suggest me to use a screen controller with a microcontroller of the STM32Lx family series or some STM32 microcontroller that has the screen driver built-in? What could you suggest me for this project? I would like the equipment to work with a 3.7v battery and use an RTOS to manage all the firmware. I almost forgot, the screen that I will use will be of the capacitive type
Thanks for the help
2023-01-26 7:15 AM
Human aspect: Need segmented, alphanumeric, pixellated display ?
Power aspect : Battery operated ?
Cost aspect : Budget ?
Performance aspect : Frames per second ? How often the screen is updated ?
2023-01-26 8:26 AM
well... I will use a pixelated display, the circuit will be powered by a 3.7V @ 4700mAh battery and I think the fps are a debatable issue, basically because if I use a tft display driver it will depend on the frequency of the communication bus and the update cycles that the uC sends, but if I use an STM32 uC that has the driver incorporated, well... I wouldn't know because I don't know how the STM32 uCs with display drivers work
2023-01-26 9:00 AM
The resolution of the display will determine the size of the frame buffer. The L4+ parts have enough internal memory for reasonably sized ones. And ones which will drive parallel TFT or MIPI-DSI screens. They don't have an FSMC to provide for external bufferring.
https://www.st.com/en/microcontrollers-microprocessors/stm32l4-plus-series.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.